The default ICS address for:
- RTAC (Comm3): 55
- 20-60 TON (Comm3): 63
- RTHD (Comm4): 65
- RTHB (Comm4): 65
- RTHC (Comm5): 65
- RTAA (Comm3): 55
- RTUA (Comm3): 55
- RTWA (Comm3): 55
- CTV (Comm4): 65
- CVHx (Comm4): 65
RTAC: The ICS address can be found through Techview. The user will go into the Configuration View and select the Options Tab. The default from the factory comes set to "default". There is a range of 1 - 64 that can be programmed. After selecting the desired address, the user should click on load configuration at the bottom of the screen.
UCP2: The ICS address can be found in Service Settings, Field Startup Group sub-menu. This menu is password protected..."+ + - - + +" "enter."
RTAA 130-400: The ICS address is accessed through the P4 menu, item 4C.
RTAA 70-125: The ICS address is accessed through Service Settings, Service Setup sub-menu. This menu is password protected..."+ + - - + +" "enter."
RTWA 70-125: The ICS address is accessed through Service Settings, Service Setup sub-menu. This menu is password protected..."+ + - - + +" "enter."
RTUA 70-125: The ICS address is accessed through Service Settings, Service Setup sub-menu. This menu is password protected..."+ + - - + +" "enter."
RTHD, CVHx: The ICS address can be found through Techview. The user will go into the Configuration View and select the Options View and make sure BAS Interface device is selected. Then go to the Options Setup View and select the correct ICS address.
Notes
- See respective IOMs for reference.
Additional details
Other Question/Problem/Cause Statements
- What is the default ICS address?
- BAS Communication Addresses?
- What is the default BAS address?
- Tracer Communication Chiller Address?
- What is the Default Chiller Address?
- Chiller Communication Address?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- CenTraVac - Direct Drive Simplex (CVHE, CVHF, CVHG)
- CenTraVac - Gear Drive (CVGF)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (PBL) (CGWD, CGWE, CGAD, CGAE, CCAD, CCAE)
- Water-Cooled Chiller (Pueblo) (CGWF, CCAF)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.