Being troubleshooting using RTAA-SB-9 or RLC-SVD03A-EN
- Disconnect heaters at E6 on 1U4. If fuse blows, then problem is with triacs or with an internal transformer within the module.
- Isolate all components and plug them in until fuse blows (divide and conquer strategy)
Additional details
Other Question/Problem/Cause Statements
- 1F15 control power fuse is blowing whenever the load triac, unload triac, or the crankcase heaters are connected.
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Crankcase heaters did not show open or shorted.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.