Compressor is starting fully loaded
- Check amp draw on startup to see if the compressor is truly starting at 100% RLA
- Check the chart in the notes section below to see how the compressor load should ramp up
- Note whether the female load stepper pulls in or not, and how fast the compressor loads up to full load.
- Compressor full load should not occur quicker that 1-2 minutes after compressor start.
- Next, use a gauge set hose to unload the male piston pressure back to compressor suction via a schrader near the male loader solenoid valves.
- If the male piston is stuck, then it can be replaced. Use RTAA-SVB-12A-EN for instructions.
- If it is the female unloader that is stuck, this cannot be easily repaired. The compressor will have to be replaced.
Notes
Additional details
Other Question/Problem/Cause Statements
- Compressor is starting up fully loaded
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.