RTWD / RTUD Chillers:
- This diagnostic is annunciated when the 115V is not seen on the 1A11 inputs through the motor thermostats
- Check thermostat wiring on terminals BT to GT; GT to RT; and RT to W
- If the 115V is not present, the 1F15 fuse could also be blown
- If the fuse is blown, both High Motor Winding Thermostat Circuit 1 and Circuit 2 will be present
- This diagnostic is valid whether the chiller is running or not
- The winding thermostat will open at 221°F and re-close at 180°F.
Notes
- This diagnostic applies to "K" and "L" frame GP2 (CHHP) compressors.
- The "M" and "N" frame compressors do not have winding t-stat.
Additional details
Other Question/Problem/Cause Statements
- High motor winding thermostat diagnostic?
- High motor temperature compressor 1A
- High motor temperature compressor 2A
- At what temperature the winding t-stat will open?
- What is the trip point for high motor temperature?
- What temperature are the Klixon thermostats set for?
- Clicks on temperature?
- ClicksOn Temperature?
- RTWD Motor Temperature diagnostic?
- What temperature does the RTWD motor temperature thermostat trip on?
- RTWD T-stat?
- RTUD T-stat?
Facts
- Water-Cooled Chiller (Pueblo) (RTWD)
- RTWD K and L compressors
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.