Scroll and Screw compressor motors are a definite purpose motor applied to Trane's specific requirements and do not fall into a NEMA classification.
In general purpose open motors, NEMA refers to a design type A, B, C or D which have to do with the motor starting current and torque characteristics.
NEMA characterizes the insulation system as to its temperature rating as classes A, B, F or H. Trane scroll and screw compressor motors use some materials that are class B in some sizes and class F in other sizes, but again does not specifically follow a NEMA requirement.
NEMA also specifies motor frame sizes and Trane scroll and screw compressors are not built at standard open motor frame sizes.
Additional details
Other Question/Problem/Cause Statements
- Compressor Motor NEMA Rating
Facts
- Air-Cooled Chiller (Pueblo) (CGAM)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Air-Cooled Chiller (Pueblo) (RTAE)
- Air-Cooled Chiller (Pueblo) (RTAF)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.