Installing External Chilled Water Setpoint to an RTAF unit requires two additional LLIDs:
- 1K24 Dual Analog I/O (Percent Capacity and Chilled Water Setpoint)
- 1K25 Dual Low Voltage Binary Input (Auxiliary Setpoint Enable)
The following changes must be made to the unit configuration using Tracer TU:
- Change External Setpoint Package to either 2-10Vdc or 4-2-mA.
Save configuration change.
Change setpoint source to EXT/FP.
The option must also be ENABLED on the TD7 as shown below:
click to enlarge click to enlarge click to enlarge click to enlarge - Go to SETTINGS...FEATURE SETTINGS...EXTERNAL CHILLED WATER SETPOINT...ENABLE...SAVE
After installing the option for ECWS, the TD7 will display an additional title for Auxiliary Chilled Water Setpoint as shown below. To eliminate this from the display, you MUST remove jumper from 1K25 J2-1 and J2-2.
click to enlarge click to enlarge click to enlarge
Additional details
Other Question/Problem/Cause Statements
- How do I add ECWS?
- How do I add External Chilled Water Setpoint?
- How do I eliminate Auxiliary Chilled Water Setpoint?
Facts
- Air-Cooled Chiller - Pueblo (RTAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.