The CGAM chiller uses CSHD and CSHN R410a scroll compressors. The compressor motors have the following electrical characteristics:
- Service factor - 1.0 (When the compressor is overloaded it will trip off)
- Maximum Acceleration time - Typical acceleration time is 0.20 seconds
- Maximum withstand time - 4 seconds (This is the maximum allowable time at LR)
Service factor, maximum acceleration time and maximum withstand time typically refer to "Open" or "TE" motors, not to specifically designed motors such as hermetic motors. This type of information is necessary when designing a starter system for a motor. The CGAM chiller is supplied with its own motor starter and protection system.
Notes
- See R-410a/R-454B CGAM Compressor sizes, quantity and model number for cross reference table of compressor model number with CGAM chiller nominal tonnage.
Additional details
Other Question/Problem/Cause Statements
- What is the service factor on the CGAM scroll compressors?
- What is the maximum acceleration time on the CGAM scroll compressors?
- What is the maximum withstand time on the CGAM scroll compressors?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.