How many starts per hour do we allow?
RTAC - Each compressor has a 5 minute start-to-start timer which prevents compressors from starting sooner. This equates to 12 times per hour, however because of EXV positioning and other timers the maximum number of starts a compressor could do would be about 10-11 per hour.
- X-line starter: 10-11 times per hour would be maximum. However, there may be excessive wear on starter components.
- Y-delta starter: the starter manufacturer recommends no more than 4 times per hour. The transition resistors need to have time for heat to dissipate.
If the chiller/compressors are starting more than this, system/application issues should be investigated.
Notes
- See Compressor Cycling for discussion on short loop applications.
Additional details
Other Question/Problem/Cause Statements
- How many starts per hour do we allow?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.