The CGAM is standard with super quiet operation with low noise fans.
The comprehensive sound attenuation package is optional. The sound attenuation package consists of sound wraps that are placed around the scroll compressors. In the engineering sound bulletin this is reflected as the "Comprehensive Acoustic Package Option."
For sound data, see CG-PRB010-EN. Sound can be found in TSA or in the sound bulletin located on E-library.
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.