What's the difference between ice-making and low temp?
RTWD/RTUD
RTWD can be used for both ice-making and low temperature process solutions. The options are selectable in TOPSS (or latest software) and the chiller will be built with HiVi compressors for high lift (vs. standard LoVi - optimized for higher efficiency at lower lift) and an oil cooler. The ice-making option will also require the ice-making LLID selected.
The RTUD is selectable in TOPSS (or latest software) with low temperature process solutions. The RTUD can also be used for ice-making, but this will require a design special.
RTUD is always built with HiVi compressors and an oil cooler.
Additional details
Other Question/Problem/Cause Statements
- What's the difference between ice-making and low temp?
- Can we change this chiller to low temperature if it was ordered for comfort cooling?
- What allows the chiller to make ice?
Facts
- Water-Cooled Chiller (Pueblo) (RTWD)
- Compressor Chiller (Pueblo) (RTUD 70-200 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.