Does the chiller ship with oil in it?
- RTHD chillers are available for order without refrigerant to facilitate disassembly and reassembly at the final installation site.
- If the chiller is ordered with a nitrogen holding charge, it will be shipped with its complete oil charge.
- It is important to note that polyester oil is hygroscopic, so it is advisable to drain all the oil and replace it with a fresh charge of oil if the unit is disassembled.
- Oil has the potential to circulate within the chiller while being transported. If the entire amount of oil is not located in the oil sump, it is recommended to inspect the condenser, evaporator, and compressor for the presence of oil.
Additional details
Other Question/Problem/Cause Statements
- Does the chiller ship with oil in it?
- When shipped with nitrogen holding charge, do it ship with oil?
Facts
- Water-Cooled Chiller (Pueblo) (RTHD)
- Shipped with nitrogen holding charge
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.