Over Current diagnostic
- Attach a gauge set hose to the Schrader near the unload solenoid valve on top of the compressor
- Vent the gauge set to the top of the evaporator
- See if the compressor unloads and when the gauge set valve is closed, will it stay in the same position
- If not successful on isolating cause, than the oil tank will have to be removed and the internal line that feeds oil to the piston cavity should be examined for cracking
- See RTHA-SB-15 for more information
- If the internal oil line is not cracked, then the piston may need replacement or rebuilt
Additional details
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.