Can I use R407C in place of R22?
In CGAF chillers, it is acceptable to use R407C as a drop in replacement. However, the mineral oil shipped with CGAF chillers (Trane Oil 42) must be removed and replaced with POE oil ( Trane Oil 78). There should not be more than 5% mineral oil content in POE oil. A minimum of 2 oil changes should be performed to remove as much of the residual mineral oil as possible.
Notes
- R407C is ONLY approved for CGAF, no Pueblo products have been tested or approved for R407C.
Additional details
Other Question/Problem/Cause Statements
- Can I replace the R22 refrigerant charge with 407C?
- Is R407C a drop in replacement for R22?
- Can I use R407C in place of R22?
- Is R407C a drop in replacement for all Trane R22 Chillers?
Facts
- CGAF
- Air-Cooled Chiller - Intellipak (CGAF)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (CCAF)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (PBL) (CGWA, CGWB, CGWC)
- Water-Cooled Chiller (PBL) (CGWD, CGWE)
- Water-Cooled Chiller (Pueblo) (CGWF)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.