RTAA 130-400 ton chillers
Replacement board is BRD01090.
Chiller programmed memory is not contained in the keypad/board. Memory is located on the main 1U1 circuit board.
Occasionally, the front panel display buttons will wear out. Often this causes the display to enter a constant "scrolling" mode. The scrolling rate is such that it appears that the display is stuck, but it is actually moving so quickly that each sample time coincides with the P0 display.
In the event that the display will not advance, the keypad can be replaced.
The keypad will also be installed on a new 1U1 module, but this is considerably more expensive.
If the chiller does not run there will be a need to change out the 1U1.
Notes
- See RTAA-SB-13 for reference on this procedure.
Additional details
Other Question/Problem/Cause Statements
- 1U1 advance display switch is not working and chiller is not operating?
- Not all the pushbuttons on the 1U1 chiller module work and the chiller will not run?
- Chiller stuck in A100?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.