What are the part numbers for the connectors and wires used on RTAA 70 to 125 control modules?
There are no wire harness available for these units. The wires are field supplied. Below are the part
numbers of the J-connectors off the modules, but you and your customer/tech will need to verify
what is needed.
The 1U1: MOD00505 supersedes to MOD01424.
See the J- connections:
- J1 = CON00577 = 2 CKT, 18 AWG, ORANGE; if it is a four connector use 2- CON00577
- J2 = NA
- J3 = CON00293 = 5 CKT, 22 AWG, RED
- J4 = CON00489 = 3 CKT, 18 AWG, ORANGE
- J5 = CON00543 = 5 CKT, 18 AWG, ORANGE
- TP1 NA
- TP2 N
If it is the J-1 connection then you need two CON00577.
- 1U2: MOD00503 supersedes to MOD01422
- MOD01422 J connections
- J1 CON00577 = 2 CKT, 18 AWG, ORANGE
- J2 N/A
- J4 CON01027 = 5 CKT, 18 AWG, ORANGE
If it is the J-1 connection then you need two CON00577.
- 1U3/1U8: MOD00504 supersedes to MOD01423
- MOD01423 J-connections
- J1 CON00577 = 2 CKT, 18 AWG, ORANGE
- J2 N/A
- J3 CON00294 = 9 CKT, 22 AWG, RED
- J4 CON00543 = 5 CKT, 18 AWG, ORANGE
- J5 CON00544 = 6 CKT, 18 AWG, ORANGE
- J6 CON00543 = 5 CKT, 18 AWG, ORANGE
- J7 CON00543 = 5 CKT, 18 AWG, ORANGE
IF it is the J-1 connection then you need two CON00577.
- 1U4, 1U5: MOD00506 supersedes MOD01425.
- J1 CON00577 2 CKT, 18 AWG, ORANGE
- J2 N/A
- J3 CON00593 3 CKT, 22 AWG, RED
- J4 CON00293 5 CKT, 22 AWG, RED
- J5 CON00289 7 CKT, 22 AWG, RED
- J6 CON00593 3 CKT, 22 AWG, RED
- J7 CON00595 9 CKT, 18 AWG, ORANGE
- J8 CON00544 6 CKT, 18 AWG, ORANGE
- The J1 connector for all these modules is part # CON00577; NOTE that this is a 2 wire.
Below are the crimping tools that are needed.
- TOL01027 Crimping Head
- TOL01028 Crimping Tool
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.