RTAC Compressor or Circuit Lockout information
Circuit Lockout - Circuit #1 and Circuit #2
- Using the TechView or KestrelView service tool, navigate to the Compressor Service View; choose the appropriate circuit control block (Circuit 1 Control or Circuit 2 Control); then select the button and change between Unlocked and Locked as needed.
- At the Local display - DynaView, select the Settings Tab. Tab down to Front Panel Circuit Lockout; choose the appropriate circuit and change between Not Locked Out and Locked Out.
Compressor Lockout - Compressor 1A, Compressor 1B, Compressor 2A, Compressor 2B
- Using the TechView or KestrelView service tool, navigate to the Compressor Service View; choose the appropriate compressor control block (Compressor 1A Control, Compressor 1B Control, Compressor 2A Control, Compressor 2B Control); then select the button and change between Unlocked and Locked as needed.
External Circuit Lockout - Circuit #1 and Circuit #2
- CH530 provides auxiliary control of a customer specified or installed contact closure, for individual operation of either Circuit #1 or #2. If the contact is closed, the refrigerant circuit will not operate.
- Upon contact opening, the refrigerant circuit will run normally. This feature is used to restrict total chiller operation, e.g. during emergency generator operations.
- Connections to the External Circuit Lockout LLID (1U5) are shown in the field diagrams that are shipped with the unit.
- These customer-supplied contact closures must be compatible with 24 VDC, 12 mA resistive load. Silver or gold plated contacts are recommended.
Notes
- See appropriate RTAC IOM
Additional details
Other Question/Problem/Cause Statements
- How to Lockout a Compressor or Circuit?
- How does the external circuit lockout work?
- How can my BAS system lock out the circuit?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.