What is the wattage on the compressor belly band heater?
- Each scroll compressor on CGAM has a crank case heater at the base of the compressor (also referred to as belly band heaters)
- For the nominal 10- and 13-ton compressors, they are 90W
- All other compressors they are 160W
- The heaters are powered by the chiller's main incoming power and stepped down with the factory installed control power transformer
- The heaters must be energized 24 hours prior to startup
Additional details
Other Question/Problem/Cause Statements
- What is the wattage on the compressor belly band heater?
- Does CGAM have crankcase heaters?
- What is the wattage for the crank case heaters?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
Document Identifier: DOC-81428
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.