Is there a part number for the female load/unload piston for GP compressor
- Female piston part number 570500130100, Piston ring X04210038010
- It is not recommended that these parts be replaced in the field.
- If they require replacement, the compressor must be replaced.
Additional details
Other Question/Problem/Cause Statements
- Need part number for female load/unload piston for GP compressor
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.