R'Newal Compressor suction screen missing
To verify the screen is present, the compressor will have to be lifted and checked.
The suction screen sits up/inside the compressor and is riveted in place with three tap rivets. If looking at the compressor and not reaching up inside or visually using a light to verify the screen is in place; a technician may think the screen is missing.
The photograph in RTHA-SB-14 of the compressor and suction screen location is deceiving, as it appears the screen fits in the suction pipe coming up from the evaporator.
Chiller can run without screen in place.
Additional details
Other Question/Problem/Cause Statements
- CHHA suction screen
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.