What compressor sizes and quantity do we use in this chiller?
This compressor information is for R410a CGAM.
Pueblo CGAM 20 to 130 scroll chillers can have one or two independent refrigerant circuits, depending on chiller size.
A refrigerant circuit consists of two scroll compressors manifolded together.
- CGAM 20 to 35 = One refrigerant circuit (2 compressors in chiller)
- CGAM 40 to 120 = Two independent refrigerant circuits (4 compressors total)
- CGAM 130 = Two independent refrigerant circuits (6 compressors total)
The table below shows the compressor size and quantity in each CGAM model.
- 60Hz available in CGAM 20 to 130
- 50Hz available in CGAM 20 to 120 ***50hz Not Available with R-454B***
| CGAM | Quantity / Size | R-410a Quantity / Model # | R-454B Quantity / Model # |
|---|---|---|---|
| 20 | 10 + 10 | 2x CSHD125 | 2x CSHE117 |
| 26 | 13 + 13 | 2x CSHD161 | 2x CSHE152 |
| 30 | 15 + 15 | 2x CSHD183 | 2x CSHE117 |
| 35 | 15 + 20 | CSHN184 + CSHN250 | CSHE177 + CSHP237 |
| 40 | 2 * (10 + 10) | 2 * (2x CSHD125) | 2 * (2x CSHE117) |
| 52 | 2 * (13 + 13) | 2 * (2x CSHD161) | 2 * (2x CSHE152) |
| 60 | 2 * (15 + 15) | 2 * (2x CSHD183) | 2 * (2x CSHE117) |
| 70 | 2 * (15 + 20) | 2 * (2x CSHD184 + CSHN250) | 2* (CSHE177 + CSHP237) |
| 80 | 2 * (20 + 20) | 2 * (2x CSHN250) | 2 * (2x CSHP237) |
| 90 | 2 * (20 + 25) | 2 * (CSHN250 + CSHN315) | 2 * (CSHP237 + CSHP297) |
| 100 | 2 * (25 + 25) | 2 * (2x CSHN315) | 2 * (2x CSHP297) |
| 110** | 2 * (25 + 30) | 2 * (CSHN315 + CSHN374) | 2 * (CSHP297 + CSHP346) |
| 120** | 2 * (30 + 30) | 2 * (2x CSHN374) | 2 * (CSHP346) |
| 130 | 2 * (25 + 20 + 20) | 2 * (CSHN315 + 2x CSHN250) | 2 * (2x CSHP237 + CSHP297) |
The R-454B compressors utilize a Variable Volume Index (VVi) compressor with 2 valves added to the top of a fixed scroll. The VVI compressor has improved performance at part loads.
Additional details
Other Question/Problem/Cause Statements
- Do we manifold compressors in the CGAM?
- Do we use individual compressor per refrigerant circuit in the CGAM?
- What compressor sizes and quantity do we use in this CGAM chiller?
- How many compressors do we use in this CGAM chiller?
- What is the compressor model used in this CGAM chiller?
- How many scroll compressors do we use in the CGAM chiller?
- What compressor size is used on this CGAM chiller?
- What is the compressor model number used in CGAM?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.