Communication Loss with Fan Control after upgrading an RTAC unit with low ambient capability.
- Communication Loss due to incorrect setting for air flow steps...see snapshot below
- Airflow Variable Speed Fan for Circuit 1 and Circuit 2 needs to be "0"
- Air Flow Step 4 for Circuit 1 and Circuit 2 needs to have a value
- The default values are likely not correct for your unit. These values must be derived from the original CH530 configuration. See example below
This should resolve the Communication Loss diagnostic
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.