RTHA/RTHB CHHA compressor
Unfortunately, the only way to repair the leak is to evacuate the compressor and remove the economizer cover and replace the sensor terminal.
Contact the Trane Parts Center for the correct replacement part, KIT02206; TEMP SENSOR REPAIR (REQUIRES Gaskets: GKT1642 FOR 130/215T OR GKT1653 FOR 255/300T OR GKT2822 FOR 380/450T).
See RLC-SG-1 for reference on access to the motor terminal / temperature sensor terminal internal to the compressor.
Motor Temperature Sensor Failure: if there are failed Motor Temperature Sensors...see e-library service bulletin RTHB-SB-9 for reference to sensor input bypass.
Notes
- Please confirm part numbers with Trane Parts.
- KIT02206 → This item is No Longer Available.
- For replacement order KIT09700 and a quantity 3 of SEN00949
- KIT02206 → This item is No Longer Available.
Additional details
Other Question/Problem/Cause Statements
- How do I repair a leaking motor winding Temperature sensor terminal?
- Leaking motor temperature sensor terminal?
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.