RTAF chillers while operating at part load, may experience harmonic noise and vibration in the discharge lines and/or oil separator.
- It has been seen that at certain compressor speeds between 1800 - 3600 RPM the vibration can exceed expected design maximums.
- If the chillers/circuits operate in this region long enough, the energy of the vibration can result in copper line fatigue failure; or oil separator material/weld failure.
- Chillers/Circuits affected by this issue:
- 3-compressor RTAF...circuit 1 & circuit 2
- 4-compressor RTAF...circuit 1 ONLY
It has been demonstrated that adding mass to the discharge lines in specific locations can minimize/eliminate the vibration energy.
- Factory, as well as field vibration testing, has identified the locations on the discharge line to place mass/weights for maximum dampening to occur.
- 3-compressor RTAF chillers will have a single weight on Circuit 1; and two weights on Circuit 2
- 4-compressor RTAF chillers will have a single weight on Circuit 1.
Shown is the view from various angles, the weight location
- 3-compressor RTAF chillers Circuit 1 & Circuit 2 Compressor 1A & 2A
- 4-compressor RTAF chillers Circuit 1 ONLY Compressor 1A
shown in RED ghost image is an approved alternate location for this weight. - ALL measurements are in mm.
mm measurement are for reference ONLY...the intent is to place the weight as close to the swedge as possible while ensuring weight ID contacts copper pipe OD entirely.
Section A-A
click to enlarge click to enlarge click to enlarge
Additional weight required on Circuit 2 of 3-compressor chillers
- 3-compressor RTAF chillers Circuit 2 Compressor 2A ONLY...additional (2nd) weight location:
mm measurement are for reference ONLY...the intent is to place the weight as close to the swedge as possible while ensuring weight ID contacts copper pipe OD entirely.
Notes
- Weight Part Number:Trane PN: KIT19176
- 4-compressor RTAF will need a single weight kit
- 3-compressor RTAF will need three (3) weight kits
- weight fastener bolt torque: 20 FT-LBS
- Thread Locker: Loctite 242 (BLUE)
- add to bolts when assembling weight KIT onto discharge line
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.