Compressor Motor Information
Pueblo rotary screw compressor motors are not standard off-the-shelf motors. They are designed and built specifically for chiller applications and as a result, do not have a standard horsepower rating.
Use the following guidelines as a general rule of thumb:
- Water-cooled application - the specific output is approximately 1 horsepower per refrigeration ton for the compressor only
- Air-cooled application - the specific output is approximately 1.35 horsepower per refrigeration ton for the compressor only
It is important to remember that the motor output will be dependent on the chiller load, building load, condensing head pressures, ambient air, and how the chiller is applied.
Additional details
Other Question/Problem/Cause Statements
- What is the horsepower of the compressor motor?
- Where can I find compressor motor curve data?
- What is the compressor horsepower?
- What is the screw compressor hp?
- What's the horse power of compressors from Pueblo?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Air-Cooled Chiller (Pueblo) (RTAC)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHD)
- Water-Cooled Chiller (Pueblo) (RTWA)
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHC)
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (RTAE)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.