This diagnostic occurs if one of the following conditions exist:
- There is an outside air temperature sensor failure or the sensor is reading incorrectly.
- Refer to CGM OA Temperature Sensor Failure for more information on this type of failure.
- The outside air temperature has fallen below the low ambient pump override temperature.
- Refer to Solution Pump ControlSolution Pump Control for more information on this pump control feature.
- Outside air temp is too low, request Solution Pump to run to keep Solution moving.
Additional details
Notes
- For description of diagnostic, refer to CG-SVP01B-EN, page 58. For further discussion also see CG-EB-82.
Other Question/Problem/Cause Statements
- Low Ambient Evaporator Solution Pump Override - What does this mean?
- Low Ambient Evaporator Solution Pump Override
Facts
- Intellipak Air-Cooled Chiller 20-60
- Air-Cooled Chiller - Intellipak (CGAC, CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.