Is an external flow switch required?
Yes, a flow switch/flow proving device and an auxiliary contact from the chilled water pump starter are required for proof of flow. Refer to RTHC-IOM-1C, page 3-10 for further information.
Additional details
Other Question/Problem/Cause Statements
- Is an external flow switch required?
Facts
- Water-Cooled Chiller (Pueblo) (RTHC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.