Why can't I get a Lo Vi compressor?
Our practice has been to provide all GP1 service compressors as Hi Vi. The reason for this is:
- A Hi Vi compressor running in a low pressure ratio application will be reliable.
- A Lo Vi compressor mistakenly put into a high pressure ratio application is at risk of failure. We didn't want to live with the risk of a mix-up.
- A Hi Vi compressor will not be quite as efficient as a Lo Vi compressor in a low pressure ratio application, but the loss is in the range of 1 or 2%.
We felt that the reliability risks more than offset the efficiency gain, so we settled on Hi Vi compressors. If the RTWA unit was new and in warranty, we had typically built a Lo Vi compressor here in Pueblo to replace any failures, but that is not an option.
Additional details
Other Question/Problem/Cause Statements
- Why can't I get a Lo Vi compressor?
- Why is the replacement compressor a Hi Vi compressor?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.