Why isn't the second compressor on each circuit coming on?
There is a KW inhibit input on the 1A7 LLID across terminals J2-3 & 4. If this input is seen open, the second compressor on each circuit will be locked out and the operating mode will be running limit; sub operating mode will be maximum capacity; compressor inhibit. This input needs to be shorted to allow the second compressor of each circuit to run.
Notes
There is another limit - Hot Start Capacity Limit - that will also keep the second compressor on each circuit from coming on. This limit is in effect whenever the evaporator leaving water temperature is above 71°F. The second compressor will remain inhibited until evaporator leaving water temperature falls below 66°F.
Additional details
Other Question/Problem/Cause Statements
- Why isn't the second compressor on each circuit coming on?
Facts
- CGWF, CCAF - CH530
- Top operating mode is Running Limit
- Sub operating mode is Maximum Capacity
- Compressor inhibit
- Compressor Chiller (Pueblo) (CCAF)
- Water-Cooled Chiller (Pueblo) (CGWF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.