Here are the basic steps to replace a damaged Dynaview controller.
There are 2 possible scenarios:
- The first one is when the touch screen is either damaged, out of calibration or non responsive but you can still connect to the controller via Kestrelview.
- The second is when you don't have access to the DV by either way and you must use the model number on the unit nameplate to re-configure the unit.
Scenario #1
Before you remove the damaged DV (Dynaview) from the unit connect to it with KestrelView (Techview)
- Click on "View" and then go to "Configuration".
- Once in configuration at the bottom of the page click on "Save to File".
-
Ensure you know where this configuration file is being saved (file path name).
- Now the complete configuration has been saved but we strongly suggest taking pictures of each configuration tab (Unit Type, CH530, Options, and Options Setup) with your phone.
- Be sure you scroll down as some of the tabs may have more information than what can be seen in the initial screen.
-
Go to “Unit View” and take a picture or write down the amount of starts and hours of each one of the compressors and water pump(s).
- You can now disconnect and remove the old Dynaview and install and the new one.
- Connect to the new Dynaview using TV.
- Got to View...Software and load the latest CGAM MP firmware version
- Once the MP is loaded it will indicate the configuration is not valid...click "Ok".
- This will take you to the "Configuration" screen.
- At the bottom of the page click on “Open from File”.
- Open the configuration file you saved from the old Dynaview.
-
Once you select it press “Load Configuration” at the bottom of the screen.
- Once the configuration is loaded use the pictures on your phone and compare all the settings.
- If any value is different, correct it to match and load the configuration again.
- The chiller is now configured.
- Now you must have KestrelView Access Level 4 for the next step.
- Go to “Unit View” and click on the “Starts and Hours” tab.
- You should be able to see and edit the white fields for starts and hours.
- Edit these values using the values on the picture you previously took.
- Finally go to “Reports” and then click on “Nameplate”.
- A Pop-up window will appear.
- Fill the model # and the Serial # from the unit nameplate.
- Once you have the correct information click on the button named “Load Unit Model Descriptor”.
- This will load and save the information.
-
If you don’t click on it the button, information will not be saved.
- Go to Binding view and validate all devices have Green Happy Faces.
- If any devices are Red Sad Face, it may require binding the device
- If any devices have a White Circles with a red X, then you need to go back to configuration and install this option
- If all devices are Green Happy Faces, the new Dynaview is now configured and ready to run
- Save the "Chiller Service Report" and "Configuration Report" to Comfortsite
Scenario #2
- Remove the old Dynaview and install the new one.
- Connect to the new Dynaview using TV and load the latest CGAM MP firmware version.
- Once the MP is loaded it will indicate the configuration is not valid.
- Click "Ok"...this will take you to the "Configuration" screen.
- Go to MNL (Model Number Lockup) on the internal "Trane Service Technicians" page and search for archived configuration files.
- If you have access to any of these files or a Chiller Service Report follow the procedure above.
- If you do not have access to a configuration file continue with the next step.
- Using the Installation, Operation and Maintenance manual (CGAM-SVX17*-EN) go to the View...Configuration tab.
- Begin selecting proper values based on the model number. Reference the IOM for clarification.
- If you are unsure, leave the setting with the default value.
- Now you must have KestrelView Access Level 4 for the next step.
- Go to “Unit View” and click on the “Starts and Hours” tab.
- You should be able to see and edit the white fields for starts and hours.
- Edit these values using the values on the picture you previously took.
- Go to Binding view and validate all devices have Green Happy Faces.
- If any devices are Red Sad Face, this may require binding the device
- If any devices have a White Circles with a Red X, then you need to go back to configuration and install this option.
- Once all devices are Green Happy Faces, exit Binding View.
- Go to “Reports” and then click on “Nameplate”.
- A pop-up window will appear.
- Fill out the model # and the serial # from the unit nameplate.
- Once you have the correct information, click on the button named “Load Unit Model Descriptor”
- This will load the information.
- If you don’t click on it the button, the information will not be saved.
- The new DV is now configured and ready to run.
Helpful Kestrelview / Techview Icons
Products Affected
- CGAM
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.