Motor terminal connectors (Spark Plugs) cracked. How are these replaced?
RTHA, RTHB Chillers/Compressors:
Refer to RTHA-SB-15 (attached below) for compressor disassembly instructions and information.
To separate the economizer cover from the motor housing:
- Choose one of the holes on the economizer cover.
- "Tap" this hole for a larger bolt ("tap" at least 1/2 the thickness of the economizer cover).
- Use this hole in a "jacking bolt" configuration to separate/pop the economizer cover from the motor housing (this is a gasket connection).
- Follow remaining procedures in RTHA-SB-15 for access to the motor terminals.
- Replace motor terminals per service guide RLC-SG-1 (attached below).
Additional details
Other Question/Problem/Cause Statements
- Motor terminal connectors (Spark Plugs) cracked. How are these replaced?
- Economizer cover removal?
- Motor Terminal Replacement?
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.