RTAC chillers:
When cleaning up system motor burns using an outside vendor/contractor it may be necessary to connect their equipment (Kidney Machine) to the chiller without a compressor connected. To facilitate this; Blank Flange plates for suction and discharge will need to be provided to they can configure some type of connection adapter.
Suction Blank
- Model N Compressor: 5702 1500 0100
- Model M & L Compressor: 5702 1500 0200
Discharge Blank
- Model M & N Compressor: X 1504 9800 000 (FLG00110)
- Flange Blanks for Hudson Technologies (www.hudsontech.com)
- Flange Blanks for CFC Refimax (www.refimax.com)
Additional details
Other Question/Problem/Cause Statements
- Flange Blanks for motor burn clean up
- Motor Burn Cleanup
- Flange Blanks for Hudson Technologies
- Flange Blanks for CFC Refimax
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.