Discharge Line Bolt Torque? What is the discharge line bolt torque?
RTHA / RTHB Chillers:
- See RTHA-SB-14 (attached below) for chiller disassembly / reassembly information. Assembly bolt torque values are in this Service Bulletin.
Notes
- See RTHA-SB-15 (attached below) for Compressor disassembly/reassembly and compressor specific bolt torque.
Additional details
Other Question/Problem/Cause Statements
- Discharge Line Bolt Torque? What is the discharge line bolt torque?
- What is the Discharge Line Bolt Torque?
- What is the bolt torque on an RTHA / RTHB chiller?
- What are the required torque values for reassembly of an RTHA chiller?
- What are the required torque values for reassembly of an RTHB chiller?
- RTHA Bolt torque values?
- RTHB Bolt torque values?
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.