Demand Limit
- Demand Limit limits the maximum number of running compressors in order to control chiller power consumption / capacity.
- DynaView / CH530 controls shall provide a means to limit the maximum number of running compressors. The maximum number of compressors allowed to run can vary from zero to the number of compressors on the unit / chiller.
- When demand limit is in effect, and the staging algorithm desires more compressors than the Active Demand Limit Setpoint will allow; an appropriate operating submode shall be displayed (Maximum Capacity).
Additional details
Other Question/Problem/Cause Statements
- How to limit the number of compressors that can run?
- Is there a way to limit the number of compressor running on this chiller?
- How do I limit the number of compressors running on this chiller?
Facts
- Air-Cooled Chiller (Pueblo) - CCAF
- Water-Cooled Chiller (Pueblo) - CGWF
- CCAF 20-60 TON chiller
- CGWF 20-60 TON chiller
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.