GP1 Male Loader/Unloader Orifice Plates
The orifice plates under the male loader/unloader valves part numbers are:
- PLT03713 ( X05140386010) → 0.0325"
- PLT03712 ( X05140386020) → 0.0255"
The smaller orifice plate goes under the male load solenoid valve, and the larger orifice plate goes under the male unload solenoid valve.
See service bulletin RTAA-SVB12A-EN (attached below) for additional information.
That plate is an orifice plate that must be kept for proper oil metering.
Additional details
Other Question/Problem/Cause Statements
- Which orifice plate goes under the solenoid valves?
- Which orifice plate goes under the load solenoid valve?
- Which orifice plate goes under the unload solenoid valve?
- Does the orifice plate between the unloader solenoid valves need to be kept or can it be discarded?
- GP1 Male Loader/Unloader Orifice Plates
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.