Compressor is loading more when the unload solenoid valve is pulsed than when the load solenoid valve is pulsed.
There are two potential causes for this problem.
- First, One of the gaskets on the discharge cover plates may be blown. It will be necessary to isolate the compressor and remove the oil filter housing and the cover plates to inspect the gaskets.
- If the gaskets are found to be ok, then a lip seal may have failed. If this is the problem, the compressor cannot be repaired and must be replaced.
Additional details
Other Question/Problem/Cause Statements
- Compressor is loading more when the unload solenoid valve is pulsed than when the load solenoid valve is pulsed.
Facts
- RTAA 70-125 TON (PUEBLO)
- Replacement compressor. Worked properly for one year. Within past two weeks, it started these symptoms.
- Verified that load and unload solenoid valves were wired correctly.
- Utilized a check for magnetism on the load solenoid when the unload solenoid was pulsed. This rules out the possibility that valves are wired such that both can be fired at once.
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.