Compressor won't load or make setpoint.
- Refer to RTHA-SB-12 for load/unload solenoid valve troubleshooting.
- Put the compressor into manual loading and check the triac output of 115V at J4-1 on the 1U2 circuit module.
- Put a hose on the oil line valve on the outlet to the oil separator tank and connect it to the schrader next to the unload solenoid valve on top of the compressor. Monitor amp draw to see if it increases.
- Check refrigerant charge to see if it is properly charged.
- Make sure all oil service valves on the compressor are open.
Additional details
Other Question/Problem/Cause Statements
- Compressor won't load or make setpoint.
- Compressor will not load up
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.