RTHB and RTHA Chillers:
- When the RTHB/RTHA compressor immediately loads up there are a couple of possible problems that could cause this.
- Verify whether the problem is electrical or mechanical.
- To check for an electrical problem, verify the load solenoid is not being continuously energized by looking at the triac output on J4-1 of the 1U2 (RTHB Circuit Module); or the 1U1-A (RTHA Relay Module).
- If the problem is mechanical, the highest probable suspect would be a fractured internal hydraulic oil line.
- To check the integrity of this line, you will first need to isolate the compressor.
- Block off the load and unload solenoid valves off with shim stock.
- By doing this, you will have isolated the piston cavity of the compressor.
- Use your manifold gauge set and pressurize the piston fitting (between the load and unload solenoid valve).
- If the pressure immediately leaks from this cavity, the oil tank will need to be removed and the line will need to be repaired.
- A worn or damaged Piston Compression Ring can also cause this same problem; verify from above whether or not the piston or hydraulic line is the issue.
Refer to RTHA-SB-12 and RTHA-SB-15 (both attached below) for additional resources, including visual aids. When oil tank is removed from compressor and the piston cavity is pressurized, you can see the pressure immediately bleed from the fracture on the line.
Changes
- Replaced load and unload solenoid valves.
Additional details
Other Question/Problem/Cause Statements
- Compressor immediately loading up?
- HPC?
- High Pressure Cutout?
- Compressor loads up right away?
- What can cause low evaporator refrigerant temperature?
- Compressor is starting up loaded?
- Failed Internal Copper Line?
- Failed Internal Copper Line (Double Flair)?
- Failed Internal Hydraulic Line?
- Failed Internal Hydraulic Line Double Flair?
Facts
- Piston ring may or may not be worn.
- RTHB 130-215 ton sizes only
- Water-Cooled Chiller (Pueblo) (RTHB)
- Water-Cooled Chiller (Pueblo) (RTHA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.