RTAA 130-400 TON Chiller:
- Used troubleshooting from RTAA-SVD01A-EN to check out compressor, possible causes:Worn Piston Rings
- Stuck Piston
- Slide Valve separated from Slide Valve Shaft
- Bronze Filters under Load/Unload Solenoid Valves plugged (Remove to correct)
Refer to RTAA-SVB09C-EN for instructions on piston replacement, attached below.
Changes
- Pulsing or continuously powering the unload solenoid valve does not unload the compressor at all.
Additional details
Other Question/Problem/Cause Statements
- Compressor will not Unload?
- Compressor will start unloaded, but loads to over 100% RLA in just a few seconds?
- HPC?
- High Pressure Cutout?
- Low Oil Flow?
- Fans not staging fast enough?
- Compressor Starts Loaded?
- Low Oil Flow...Diagnostic 198?
- Low Oil Flow...Diagnostic 199?
- Compressor Starts Loaded Intermittently?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 130-400 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.