Make sure to properly identify the unload and load solenoid valves when re-wiring after an R-Newal. Refer to RTHA-SB-12, page 2 for a picture of the solenoid valve locations. Note that the schraeder valve is always closest to the unload solenoid valve.
Additional details
Other Question/Problem/Cause Statements
- Compressor will not load.
Facts
- Compressor has just gone through an R-Newal and the solenoid valves had to be re-wired.
- Water-Cooled Chiller (Pueblo) (RTHA)
- Water-Cooled Chiller (Pueblo) (RTHB)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.