CGAM Chillers utilize an Efector Flow Switch. There are 3 LEDs on the flow switch cable.
- Green LED ON indicates Power and Flow.
- Amber LED & Green LED ON indicates NO Flow.
- Two Amber LEDs & Green LED ON indicated No Flow and possible wiring error.
- Amber LED & NO Green LED... not possible unless the Cable is Bad or there is a wiring error.
CGAM ships standard with an IFM efector flow switch. Paddle style flow switches are not available as an option.
The CGAM can ship with 4 different flow switch set points which are determined by design conditions.
LWTE, Glycol type and percentage of glycol will determine flow switch set point. Flow switch set point is an output in TOPSS output. It can be found in the "General' section.
- SENSOR: FLOW SP=15CM/S
- SENSOR: FLOW SP=35CM/S
- SENSOR: FLOW SP=45CM/S
- SENSOR: FLOW SP=60CM/S (all unit with water only)
Additional details
Other Question/Problem/Cause Statements
- Efector Flow Switch LED Indication?
- LED Color indicating Flow when using an Efector Flow Switch?
Facts
- Air-Cooled Chiller (Pueblo) (CGAM 20-130 Ton)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.