What low pressure controls have to be changed when converting a CGAF to low leaving water temperature?
The following parts can be used to modify a unit in the field from a factory ordered leaving water temperature to a lower leaving water temperature. It is recommended all changes are verified through the Field Modifications Group in La Crosse.
Plate and Frame Evaporator
THESE MECHANICAL MODIFICATIONS APPLY ONLY TO CGAF CHILLERS WITH PLATE AND FRAME EVAPORATORS.
The system must have appropriate amount of Glycol to run at low temperatures.
| 20 ton | 25 ton | 30 ton | |
|---|---|---|---|
Digit 11 = E or 4 20-29°F Leaving Water Temp | Replace expansion valve with X15110392-07 OVEN15-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-21, 20 psig | Replace expansion valve with X15110392-07 OVEN15-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-21, 20 psig | Replace expansion valve with X15110389-07 OVEN20-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-22, 20 psig |
Digit 11 = B or 2 30-39°F Leaving Water Temp | Replace expansion valve with X15110392-07 OVEN15-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-21, (Digit 11 = 2) 20 psig Low Pressure Control X13200053-25, (Digit 11 = B) 25 psig | Replace expansion valve with X15110392-07 OVEN15-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-21, (Digit 11 = 2) 20 psig Low Pressure Control X13200053-25, (Digit 11 = B) 25 psig | Replace expansion valve with X15110389-07 OVEN20-N High pressure cutout switch - X13210029-19, 360 psig Low Pressure Control X13200053-22, (Digit 11 = 2) 20 psig Low Pressure Control X13200053-26, (Digit 11 = B) 25 psig |
| 40 ton (qty2) | 50 ton (qty2) | 60 ton (qty2) | |
Digit 11 = E or 4 20-29°F Leaving Water Temp | Replace expansion valves with X15110392-11 OVE15-N High pressure cutout switches Low Pressure Controls X13200053100, | Replace expansion valves with X15110392-11 OVE15-N High pressure cutout switches Low Pressure Controls X13200053100, | Replace expansion valves with X15110392-12 OVE20-N High pressure cutout switches
|
Digit 11 = B or 2 30-39°F Leaving Water Temp | Replace expansion valves with X15110392-11 OVE15-N High pressure cutout switches Low Pressure Control X13200053-21, (Digit 11 = 2) Low Pressure Control X13200053-25 (Digit 11 = B), | Replace expansion valves with X15110392-11 OVE15-N High pressure cutout switches Low Pressure Control X13200053-21, (Digit 11 = 2) Low Pressure Control X13200053-25 (Digit 11 = B), | Replace expansion valves with X15110392-12 OVE20-N High pressure cutout switches Low Pressure Control X13200053-21, (Digit 11 = 2) |
Shell and Tube
THESE MODIFICATIONS APPLY TO CGAF CHILLERS WITH SHELL AND TUBE EVAPORATORS.
The system must have appropriate amount of Glycol to run at low temperatures.
| 20 ton | 25 ton | 30 ton | |
|---|---|---|---|
size=2> 20-29 F Leaving Water Temp | Replace expansion valve with OVE15-N High pressure cutout switch Low Pressure Control X13200053100, 20-35 psig | Replace expansion valve with OVE15-N High pressure cutout switch Low Pressure Control X13200053100, 20-35 psig | Replace expansion valve withOVE15-N High pressure cutout switch Low Pressure Control X13200053100, 20-35 psig |
size=2> 30-39 F Leaving Water | Replace expansion valve with OVE15-N High pressure cutout switch Low Pressure Control X13200053150, 25-40 psig | Replace expansion valve with OVE15-N High pressure cutout switch X13210094-01, 360 psig Low Pressure Control X13200053150, 25-40 psig | Replace expansion valve withOVE20-N High pressure cutout switch X13210094-01, 360 psig Low Pressure Control X13200053150, .25-40 psig |
size=2> 40 ton (qty 2 ) | size=2> 50 ton (qty 2) | size=2> 60 ton (qty 2) | |
size=2> 20-29 F Leaving Water Temp | Replace expansion valves with OVE15-N High pressure cutout switches Low Pressure Controls X13200053100, 20-35 psig | Replace expansion valves with OVE15-N High pressure cutout switches Low Pressure Controls X13200053100, 20-35 psig | Replace expansion valves with OVE15-N High pressure cutout switches Low Pressure Controls X13200053100, 20-35 psig |
size=2> 30-39 F Leaving Water Temp | Replace expansion valves with OVE15-N High pressure cutout switches Low Pressure Controls X13200053150, 25-40 psig | Replace expansion valves with OVE15-N High pressure cutout switches Low Pressure Controls X13200053150, 25-40 psig | Replace expansion valves with OVE20-N High pressure cutout switches Low Pressure Controls X13200053150, 25-40 psig |
Additional details
Facts
- Air-Cooled Chiller - Intellipak (CGAF)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.