HPCO
RTHB
RTHA
HPC
High Pressure
- The high pressure switch (HPC) is set at 90% of the high side relief valve.
- The relief valve on RTHB is 300psi, therefore, the HPC is 270 psi.
- There is a setting in the Machine Configuration Group for High Pressure Cutout Setting.
- The value of this setting will determine when the chiller will go into condenser limit mode.
- The HPC is a mechanical switch and has no correlation to this setting.
Notes
- Not until March of 1997 was a Schrader valve installed underneath the HPC
Additional details
Other Question/Problem/Cause Statements
- What is the High Pressure Cutout?
- What is the HPC trip point?
- What pressure does the HPC trip at?
- What pressure does the High Pressure Cutout Trip at?
- At what point does the High Pressure Cutout open?
Facts