What does it take to convert a 460V/60Hz/3 to 400V/50Hz/3?
In general, the RTAC's are not able to be converted from 460V/60Hz/3 to 400V/50Hz/3. This affects more than the electrical, but also the capacity.
Other Question/Problem/Cause Statements:
- What does it take to convert a 460V/60Hz/3 to 400V/50Hz/3?
- Conversions from 50Hz to 60Hz
- Can you offer a 50Hz voltage RTAC model 450 or 500?
Additional details
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.