Can I convert the RTWD chiller from R134a to R513a refrigerant?
For RTWD package unit, replacing R134a with R513A is a relatively easy process.
- What parts need to be changed out?
- Just refrigerant
- Limitations imposed
- ONLY can be applied to certain selected chiller configurations.
- Different lubricant / oil? *** read additional comments under NOTES ***
- Same oil
- Does the refrigerant system need to be cleaned/flushed before putting new oil and R513A refrigerant
- No, R513A is compatible with R134a
- Do we have a need to install new MP Software in the DynaView Controls for R513A; and does the Trane technician have to manually change the settings/safeties?
- Yes, the Controls MP Software will need to be updated to the latest version in KestrelView/TechView v15.0; and the configuration will need to be updated to show R513A – utilizing slightly different properties and control algorithms.
Notes
- R513A can ONLY be applied with RTWD chillers that have Hi-Vi compressors installed.
- Low Temperature Process selected chillers.
- High Condensing Temperature or Hot Water Control selected chillers.
- RTWD standard application with Low-Vi compressors and current chiller controls could compromise compressor and chiller reliability due to superheat limitation and lubrication/oil-return and oil quality issues.
Additional details
Other Question/Problem/Cause Statements
- What is necessary to convert an RTWD charged with R134a to R513A?
- Can this chiller be converted to R513A?
- Is RTWD convertible and compatible with R513A refrigerant?
- Is RTUD convertible and compatible with R513A refrigerant?
- Low GWP options for RTWD chillers?
- Low GWP options for RTUD chillers?
- Low GWP conversion option for RTWD?
- Low GWP conversion option for RTUD?
Facts
- Water-Cooled Chiller (Pueblo) (RTWD)
- Air-Cooled Chiller (Pueblo) (RTUD)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.