All of our Direct Expansion (DX) Evaporators use Profax 6823 plastic, a polypropylene derivative, for the baffles. For this reason we do not recommend excess of 108°F water through the evaporator, which could cause failure to these baffles.
Maximum Evaporator Temperature = 108°F
Additional details
Other Question/Problem/Cause Statements
- Evaporator Baffles
Facts
- CGWA, CGWB, CGWC, CGWD, CGWE, CGWF, CCAF
- RTAA 70-125 Ton (Pueblo)
- RTUA
- RTWA
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.