RTHA Chillers: Low Pressure Cutout
- Low Pressure Cutout (1TB3-24, -25)
- These terminals monitor the pressure in the evaporator. If the pressure falls below 45 +/- 10 psig for design Sequence A thru E closure of 4S6 between 1TB3-24 and 1TB3-25 will shut down the unit giving a latching diagnostic (b b5). For design sequence F and on, the low pressure cutout is 26 +/- 10 psig.
- The LPC input is a Normally Open Input (module logic).
- When the chiller has refrigerant in it, the LPC switch is OPEN; when there is loss of charge the switch CLOSES (close on Low Pressure) generating a latching Low Pressure Cutout (b b5).
- This could be caused from catastrophic loss of charge or a faulty low pressure switch.
- Use gauge to verify pressure in the evaporator if this diagnostic cannot be cleared.
Notes
- Observe the gender (Normally Closed) of this switch; it is different than other switches used in this capacity (Normally Open, which open on a fault rather than close).
Additional details
Other Question/Problem/Cause Statements
- b5...Low Evaporator Refrigerant Pressure?
- Low Pressure Cutout?
- Low Pressure diagnostic?
- Low Pressure?
- LPC?
Facts
- Water-Cooled Chiller (Pueblo) (RTHA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.