Are the oil separator heaters in wells?
RTAC Chillers:
- Design Sequence A0 & B0 → heaters are NOT in wells.
- Design Sequence C0 + → heaters are IN wells.
- Design Sequence digits are 10-11 of the model number.
Additional details
Other Question/Problem/Cause Statements
- Are the oil separator heaters in wells?
- The oil separator heater shorted to ground...Is this heater in a well?
- When were heaters put into the oil separator wells on RTAC?
Facts
- Air-Cooled Chiller (Pueblo) (RTAC)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.