There are two orifice plates (one marked 32 and the other marked 25) below the unload and load solenoid valves
- The one marked 32 is installed below the unload solenoid valve which is the closest solenoid valve to the discharge end of the compressor
- The one marked 25 is installed below the load solenoid valve
- Both numbers showing be installed toward the outside of the compressor
Additional details
Other Question/Problem/Cause Statements
- There are two orifice plates (one marked 32 and the other marked 25) below the unload and load solenoid valves. Which one goes where?
- What is the metal between the gaskets under the load and unload solenoids?
- What is the correct location of the 32 and 25 orifice under the solenoids?
Facts
- Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.