There is a bolt on the side of the compressor near the motor that is leaking. What is this?
This is the motor stator locking bolt.
- It is there to lock in the motor stator and keep it from rotating.
- It has an o-ring that can be replaced.
Additional details
Facts
- RTAA 70-125 TON (PUEBLO)Air-Cooled Chiller (Pueblo) (RTAA 70-125 Ton)
- Compressor Chiller (Pueblo) (RTUA)
- Water-Cooled Chiller (Pueblo) (RTWA)
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.