RTAC chillers operating in various applications, under various conditions; exhibiting intermittent Liquid Level Sensor (LLS) abnormalities...resulting in various diagnostics:
- Pump Down Terminated
- Low Evaporator Temperature...Unit Off - Circuit 1 / 2
- Operational Pump Down into a vacuum
- Evaporator Refrigerant Drain - Circuit 1 / 2 ( Remote Evaporator Chillers ONLY )
- Low Suction Refrigerant Pressure - Circuit 1 / 2
- High Evaporator Refrigerant Pressure
- High Evaporator Water Temperature
Modification Parts KITs:
There are 4 kits available, depending on the specific RTAC chiller size and efficiency/performance configuration:
- KIT 17875 - 2 compressor140 TON STD, 120 TON HIGH
- 155 TON STD, 130 TON HIGH
- KIT 17964 - 2 compressor170 TON STD / 140 TON PREM
- 185 TON STD
- 155 TON PREM
- 200 TON STD
- 170 TON PREM, 140 TON XE 60 HZ
- 225 TON STD 60 HZ
- 185 TON PREM / 155 TON XE 60 HZ
- 250 TON STD 60 HZ / 200 TON PREM / 170 TON XE 60 HZ
- 225 TON HIGH / 250 TON HIGH 60HZ, 185, 200 TON XE 60 HZ
- KIT 17876 - 3 compressorAll units with 3 compressors
- KIT 17877 - 4 compressorAll units with 4 compressors
- HUS 04208:
- HOUSING, SPECIALTY, LIQUID LEVEL SENSOR
- If there is a field requirement to replace a damaged RTAC Top-down LLS Canister (DO NOT ORDER THIS PART FOR FIRST TIME INSTALLATION)
- SEN 01552 - LIQUID LEVEL SENSOR; 3.54" [90MM] , TOP MOUNT
Procedure Outline
- Follow proper LOTO for chiller and/or circuit as required.
- Isolate evaporator by closing the appropriate refrigerant/oil isolation valves.
- Recover ALL refrigerant/oil from the affected circuit evaporator.
- Remove existing Liquid Level Sensor (LLS) canister and lines.
From modification KIT...install the new top mounted LLS canister and lines.
- From modification KIT...install new 90MM top mounted LLS.
- Using TechView/KestrelView, make a local connection to the chiller controller (DynaView).
- Select View \ Software...select Product 'RTA'; select Available Version 46.0 or newer (if not already installed).
- Select 'Download Software to Main Processor'...
- Once the correct MP software is loaded on the DynaView, if not already connected locally, make a local connection to the chiller controller (DynaView)
- Select View \ Configuration \ Custom \ Circuit 'X' Liquid Level Sensor Type: X13790508 (90 mm Top Mount Sensor)
- Next choose the 'Load Configurations' tab at the bottom of the screen to load the new configuration.
- Loading the new configuration will result in TechView advancing to the 'Binding' process. Once in BindingView, select and BIND in the new LLS to the appropriate circuit LLS LLID.
- Exit BINDING back to UnitView. Make sure there are not active diagnostics with the LLS.
- Pressure test evaporator.
- Evacuate and perform a rise test.
Open up refrigerant/oil valve, and re-charge as necessary.
Additional details
Facts
- RTAC Liquid Level Sensor Top-Mount Retrofit
WARNING:
Information in this article is intended for use by individuals possessing adequate backgrounds of electrical and mechanical experience and who comply with all federal, state, and local laws, rules, orders, or regulations related to the installation, service, or repair of a heating or central air conditioning product. Any attempt to install, service, or repair a heating or central air conditioning product may result in personal injury and/or property damage. The manufacturer or seller cannot be responsible for the interpretation of the information contained herein, nor can it assume any liability in connection with its use.